web counter

How to Design a High-precision ADC?

Published: 13 December 2021 | Last Updated: 13 December 20212813
This article describes how to design a high precision analog to digital converter ADC, mainly including what is ADC, how to design and optimize ADC and ADC drive design.
In this video series we look at ways or tips to improve ADC measurement accuracy and resolution.

Tips on Improving ADC Measurement Accuracy and Resolution


Catalog

1. What is ADC?

2. How to design and optimize ADC?

3. ADC drive design

 

1. What is ADC?

Essentially, the main difference between analog chips and digital chips is the difference in signal processing. As the name suggests, analog chips process analog signals, while digital chips process digital signals. The analog signal changes continuously over time, such as temperature, humidity, sound, speed, and so on. Their biggest feature is that there are countless different values within a certain time range.

In contrast, a digital signal is a bunch of discrete values, such as the binary 0101 used in computers. Since the transistor has two states of on and off, it can naturally represent the values of 0 and 1. There is no way for a transistor to achieve a state like 10% on or 31.5% off, so it is a digital signal.

In order to connect the two independent fields of analog and digital, it is necessary to use two kinds of chips as a bridge, one is the analog-to-digital conversion chip ADC, and the other is the digital-to-analog conversion chip DAC.

As the name implies, the analog-to-digital conversion chip ADC is used to convert analog signals into digital signals, and the analog-to-digital conversion DAC is just the other way round, converting digital signals into analog signals. However, in practical applications, ADC accounts for a higher proportion. Data shows that 80% of the applications where analog-to-digital conversion is applied are ADCs. Especially in the digital society, almost everything has been digitized, which is convenient for subsequent processing, transmission, and storage.

Many people may think that it is not difficult that the analog signal to be converted into a digital signal. In fact, the ADC is the most difficult analog chip. At the top conference ISSCC in the field of semiconductors and integrated circuits, that is, the International Solid-State Circuits Conference, there are quite a few articles on ADC design.

2. How to design and optimize ADC?

So, how exactly is the ADC implemented? Simply put, several processes such as sampling, quantization, and encoding are required. In other words, we first need to sample this signal and record the voltage value of the signal at regular intervals. The collected value will be quantized, converted into the corresponding digital signal value, and finally expressed by some kind of code, such as complement code, gray code, and so on.

ADC has many parameter indicators, of which there are two common parameters, one is ADC sampling rate or data rate, and the other is resolution. The sampling rate is well understood, that is, how many samplings can be done per unit time, and the more sampling points, the better the original signal can be restored.

Resolution is defined as the smallest change in the value of the input signal. This smallest change in value will change a code value of the ADC digital output value. In the case that the ADC has the same input range, the higher the resolution, the smaller the minimum change represented by a code value. If an ADC has 3 bits, then the entire voltage range can be divided into 2^3=8 parts. If the voltage range is 0-10V, then each part represents 1.25V. In other words, if the voltage change is less than this value, then the ADC cannot capture this small change. The important thing to note is that ADC resolution and ADC accuracy are two completely different concepts.

ADC code.jpg

ADC code

There are many specific implementation forms of ADC, the common ones include successive approximation ADC (SAR), and there is also a Delta-Sigma ADC. For example, a common successive approximation ADC mainly integrates a voltage comparator, a register, a DAC, and some control circuits in the circuit. Its essence is to use binary search to determine the digital signal corresponding to the analog voltage. That is, in the beginning, the input voltage is compared with half of the reference voltage. If the input voltage is larger, then compare with three-quarters of the reference voltage. On the contrary, if the input voltage is smaller, it is compared with a quarter of the reference voltage. And so on, until the comparison is complete.

3. ADC drive design

However, even the most basic ADC is not simple in actual engineering applications, so supporting resource is particularly important. For example, ADCs often cannot work independently. They need to cooperate with other external circuits to function. One of the most important external circuits is the drive circuit.

As mentioned earlier, the ADC needs to sample, quantize and encode the input signal, and output an N-bit digital signal. These operations are usually completed in one cycle of the digital clock. This means that during the sampling process, the input signal should remain unchanged. This is a bit similar to the hold time of a clock in a digital signal.

Inside the ADC, its input actually contains a switch and a capacitor array, which is usually equivalent to a switch and a sampling capacitor. When the switch is closed, the capacitor is charged. After it is charged, the switch is opened, and the comparator and the DAC cooperate with each other to complete the sampling and quantization operation of the ADC at this time.

There are some problems. First of all, if the performance requirement of the ADC are relatively high. For example, if its sampling frequency is required to be high, then the time to charge the capacitor inside the ADC will be very short. If the sampling frequency is 1 million samples per second, then the charging time, that is, the capture time (TACQ) may only be 300 nanoseconds. If no circuit is added to the input as a driver, it will basically not be able to meet the demand for such a high sampling frequency. So in response to this problem, we usually add an operational amplifier to the ADC front end as a driver, so that sufficient charge can be provided to the sampling capacitor within a short sampling time.

This is not over yet. Although we can directly connect the op amp and ADC directly, we rarely design this way in practical applications. Because when the sampling frequency is very high, a very high bandwidth op amp is required if it is directly connected to the op amp. In addition, as can be seen from the simulation, the initial conversion may generate a large transient current when switching, and the driver circuit needs to be able to charge the ADC's internal sampling capacitor within a short ADC capture time (TACQ).

ADS7042 circuit.jpg

ADS7042 circuit

In order to meet these conditions and avoid large instantaneous currents, we can add an RC circuit before the ADC. We have learned in the university that the RC circuit is used for filtering, but its main function here is to use this extra capacitor to achieve faster charging. The op amp can fill this capacitor, and then when the ADC internal switch is closed, charge the ADC internal capacitor through this capacitor. Of course, in addition to this capacitor, part of the charge also comes from the front-end op amp. This RC circuit is also called a charge bucket filter circuit, which can effectively reduce the bandwidth requirements of the front-end op amp, so we can choose a lower bandwidth and lower cost ordinary op amp to meet the design needs. At the same time, it also eliminates the initial instantaneous current and greatly improves the stability of the circuit.

Here comes another question. How to determine the specific size and indicators of these amplifiers and RC circuits? There are two methods here, one is to derive through theoretical formulas, this is a very detailed derivation process on the Internet. According to the ADC indicators, such as resolution, sampling rate, reference voltage, etc., you can derive the required RC circuit and op-amp parameter data step by step.

Of course, there is another method, which is to perform simulation calculations through ready-made design tools and simulation tools. For example, Texas Instruments TI provides a series of related tools to simplify all the above calculation processes. In the beginning, you can select the corresponding device according to the performance indicators of the ADC, and then use the ADC SAR Drive tool to directly calculate the value of the resistance and capacitance, and get the corresponding performance indicators.

In order to further simplify the design process, TI not only provides design tools, but also a complete ecosystem to integrate these tools.

TI circuit cookbook.jpg

TI circuit cookbook

Taking SAR drive design as an example, TI provides many classic ADC circuit design solutions. For example, this "high-voltage battery monitor circuit" teaches us step by step from design description goals, to how to choose suitable devices, and how to model and simulate, and get the ideal performance index.


*This article was translated from: https://mp.weixin.qq.com/s/4r69kgCY5p1gOZnlEAd8CA

UTMEL

We are the professional distributor of electronic components, providing a large variety of products to save you a lot of time, effort, and cost with our efficient self-customized service. careful order preparation fast delivery service

Frequently Asked Questions

1. How does ADC convert analog to digital?

ADCs follow a sequence when converting analog signals to digital. They first sample the signal, then quantify it to determine the resolution of the signal, and finally set binary values and send it to the system to read the digital signal. Two important aspects of the ADC are its sampling rate and resolution.

2. How do you convert analog to digital?

If the two resistors are of equal values, that is R1 = R2, then clearly the reference voltage level will be equal to half the supply voltage, or V/2. So for a comparator with an open-collector output, if VIN is less than V/2, the output is HIGH, and if VIN is greater than V/2, the output is LOW acting as a 1-bit ADC.
Related Articles

  • Discovering New and Advanced Methodology for Determining the Dynamic Characterization of Wide Bandgap Devices
    Discovering New and Advanced Methodology for Determining the Dynamic Characterization of Wide Bandgap Devices
    Saumitra Jagdale15 March 20242928

    For a long era, silicon has stood out as the primary material for fabricating electronic devices due to its affordability, moderate efficiency, and performance capabilities. Despite its widespread use, silicon faces several limitations that render it unsuitable for applications involving high power and elevated temperatures. As technological advancements continue and the industry demands enhanced efficiency from devices, these limitations become increasingly vivid. In the quest for electronic devices that are more potent, efficient, and compact, wide bandgap materials are emerging as a dominant player. Their superiority over silicon in crucial aspects such as efficiency, higher junction temperatures, power density, thinner drift regions, and faster switching speeds positions them as the preferred materials for the future of power electronics.

    Read More
  • Applications of FPGAs in Artificial Intelligence: A Comprehensive Guide
    Applications of FPGAs in Artificial Intelligence: A Comprehensive Guide
    UTMEL29 August 20255726

    This comprehensive guide explores FPGAs as powerful AI accelerators that offer distinct advantages over traditional GPUs and CPUs. FPGAs provide reconfigurable hardware that can be customized for specific AI workloads, delivering superior energy efficiency, ultra-low latency, and deterministic performance—particularly valuable for edge AI applications. While GPUs excel at parallel processing for training, FPGAs shine in inference tasks through their adaptability and power optimization. The document covers practical implementation challenges, including development complexity and resource constraints, while highlighting solutions like High-Level Synthesis tools and vendor-specific AI development suites from Intel and AMD/Xilinx. Real-world applications span telecommunications, healthcare, autonomous vehicles, and financial services, demonstrating FPGAs' versatility in mission-critical systems requiring real-time processing and minimal power consumption.

    Read More
  • The 2026 Engineer’s Guide: Choosing the Right MCU for Your Next IoT & New Energy Project
    The 2026 Engineer’s Guide: Choosing the Right MCU for Your Next IoT & New Energy Project
    UTMEL30 April 20262139

    A comprehensive comparison of 2026's leading MCUs from ST, NXP, and Microchip across power efficiency, processing performance, connectivity, and ecosystems to help engineers select the optimal chip for next-gen IoT and new energy projects.

    Read More
  • AI Server Components: Engineering Next-Gen Data Center Hardware for 100kW Racks
    AI Server Components: Engineering Next-Gen Data Center Hardware for 100kW Racks
    UTMEL15 May 20261128

    The transition from traditional enterprise IT to AI-driven workloads has rendered legacy data center hardware obsolete, forcing infrastructure planners to re-engineer server components for extreme thermal environments.

    Read More
  • The Practical Engineer’s Guide to the NE555N Timer: Pinout, Setup, and Troubleshooting
    The Practical Engineer’s Guide to the NE555N Timer: Pinout, Setup, and Troubleshooting
    UTMEL29 May 2026981

    This comprehensive guide explores the NE555N timer, detailing its 8-pin layout, internal architecture, and key datasheet specifications. It compares the bipolar IC to CMOS variants and details setup configurations for astable, monostable, and bistable modes. Additionally, the guide offers practical troubleshooting advice to prevent common breadboard failures, such as floating reset pins and electrical noise issues.

    Read More

Subscribe to Utmel !

Featured Parts More